9/7/2020 12:00 PM | |
Joined: 6/27/2016 Last visit: 7/5/2023 Posts: 33 Rating:
|
Hi, I am trying to investigate an issue with our PLC system, Different IO racks seem to drop from the profinet network then return, how ever, when looking at the diagnostics buffer for the PLC I can only see the profinet stations return and lots of IO access reading/writing errors. Is there anyway of removing these from the diagnostics buffer so I can see the original faults? I have attached diagnostics buffer Thanks Tom Varker Attachment07092020 - 1029.doc (192 Downloads) |
Follow us on