10/11/2020 7:57 PM | |
Joined: 3/28/2015 Last visit: 11/7/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topic might help: Visualization with user-defined web pages on SIMATIC CPUs with PROFINET interface ---------------------------------------------------------------------------------------------------- SIMATIC CPUs with PROFINET interface provide the opportunity to access variables of the CPU with the help of web pages provided by the system. The integrated web server of the S7-CPU is accessed via a standard web browser: To create your individual web page (user-defined web page), you can use any tools such as Microsoft Frontpage, Notepad, etc.. For designing your web page, you can use all options provided by HTML, CSS and JavaScript. In addition, there is a special command syntax (AW P command) for directed communication with the CPU. ------------------------------------------------------------------------------------------------------ |
Eng.Mohamed Ibrahim |
|
Follow us on