11/25/2020 12:07 AM | |
Posts: 2 Rating: (0) |
Is there possibility to transfer from one PLC to another safety digital I/O? For example, safety output in one PLC is Q500.0, this can be read in the other PLC as I500.0? In my case it doeasn't work, this is not supported by application or I did something wrong? Also I did transfer ProfiSAFE telegram word from one PLC to other to simulate drive safety reaction, and there was no problem, but digital safety I/O doesn't work. Best regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/25/2020 10:12:53New subject after splitting |
|
11/26/2020 8:09 AM | |
Joined: 6/19/2017 Last visit: 5/6/2024 Posts: 7996 Rating: (163) |
Closed cause question posted twice. The second thread with the subject Can the safety output from one PLC in another PLC be read via crosslink application? is published within the conference Virtual Commissioning. Best regards,Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on