2/25/2021 3:44 PM | |
Joined: 10/10/2005 Last visit: 8/29/2024 Posts: 1917 Rating:
|
Hello Petkevych, the firmware version is part of the CPU and you can find the download in the Siemens network. It also makes no sense to export the firmware from CA01, as the current firmware is always available on the Internet. There is also a description of how to proceed. An example for the firmware of an S7-300: Firmware updates for CPU 315-2 PN/DP (6ES7315-2EH14-0AB0) With best regards |
3/2/2021 1:48 PM | |
Posts: 7 Rating:
|
I try to use TIA Openness to add hardware to my project. In one side one of the parameters of program is Type identifier which contain article number and firmware version. In other side electrical drawing don't contain firmware version. So I need some database which include article number and firmware version for my TIA Openness program. The goal is that the user make's list of hardware and the program substitute firmware version automaticly how it work's on TIA Portal.
|
Follow us on