3/20/2024 8:15 AM | |
Joined: 2/28/2024 Last visit: 4/24/2024 Posts: 13 Rating: (0) |
Hello ! The TEA1, TEA2, TOA, ZOA programs are easily transferred, the file type appears in DATENART. The @@@ST.S5D file can also be loaded only with STEP5 (nothing appears in DATENART). The same S5D file written in ASCII and the other similar files are transferred by PCIN (nothing appears in DATENART), but they are not saved, I tried DATA OUTPUT and got the confirmation. The same thing happens at different transfer rates 300 BAUD or 9600 BAUD . I don't want to upset you, the last reload was done on interface 2, the person who did the reload said it's better that way, no transmission errors occur, he changed a line of bits to activate interface 2, change 2 appeared on the monitor up and 1 down, with the mention that I use interface 1 only for transmitting work programs. AttachmentImages.zip (9 Downloads) |
Last edited by: Jen_Moderator at: 03/20/2024 13:13:25Text formatting optimized. Last edited by: Jen_Moderator at: 03/20/2024 13:15:38All files added as .zip file. |
|
3/21/2024 7:34 AM | |
Joined: 2/28/2024 Last visit: 4/24/2024 Posts: 13 Rating: (0) |
Hello ! Thank you for your patience and help! I respected and followed the steps recommended by you. In the initial mode I transferred the TEA1 and TEA2 files (with the setting 5016=00101000 otherwise it does not work), I reset the power off/on and returned to the initial mode. With the setting 5010=00000100 I transferred with Step 5 the file @@@s5D. Continuing with PCIN with the same setting I tried to transfer the other files written in ASCII, PCIN shows that it is fully transferred, but it seems that they are not saved in the machine computer .The control panel of the machine has all the active functions, but the automation does not start. Attachmentfiles.zip (17 Downloads) |
Last edited by: Jen_Moderator at: 03/22/2024 05:25:08Text formatting optimized. All files added as .zip file. Last edited by: Jen_Moderator at: 03/22/2024 05:25:37Attachment added again. |
|
Follow us on