4/23/2024 3:14 PM | |
Joined: 4/23/2024 Last visit: 4/24/2024 Posts: 2 Rating: (0) |
When I uninstalled TIA Portal V18,then install TIA Portal V17,It appeared. It said "stuck in ClassicCompPrepare",that all i knew. AttachmentSIA_STEP7_S7FPLUS_WINCC_PRO_V17@24-04-23_22-40-29.txt (8 Downloads) |
4/24/2024 4:57 AM | |
Joined: 4/23/2024 Last visit: 4/24/2024 Posts: 2 Rating: (0) |
It didn't work.I also uninstalled SQL,still not workout. |
4/24/2024 5:22 AM | |
Joined: 3/11/2019 Last visit: 5/21/2024 Posts: 1425 Rating: (257)
|
Hi, seems like the FAQ was taken offline, at least the link to the FAQ do not work anymore (following from older posts, the FAQ was mentioned). But as far as I can remember, the uninstallation process was done via the inventory tool. https://support.industry.siemens.com/forum/de/en/posts/how-to-uninstall-tia-portal-v16-/252821 https://support.industry.siemens.com/forum/de/en/posts/complete-uninstall-of-tia-v13-sp1/159409 But i agree, a Support Request is the probably the way to go. And you can collect the systems diagnostic data directly and provide it to the technical support. Most likely this is the first thing which is aked for... SIMATIC Assessment Suite - Data Collector (SAS-DC): Download and Instructionsregards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to2 thankful Users |