5/26/2006 8:17 AM | |
Posts: 10 Rating: (0) |
how can I get a manual of FM352-5? and how can I update the hardware catalog in step7?[:)]I |
5/26/2006 6:57 PM | |
Joined: 9/23/2005 Last visit: 9/17/2024 Posts: 4347 Rating: (1446) |
Hi, the manual of CP352-5 stay in the link: http://support.automation.siemens.com/WW/view/en/9240171 and the configuration pacage can be order with the number: 6ES7 352-5AH00-7XG0 |
Denilson Pegaia |
|
5/26/2006 8:42 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318) |
Hi Zhao, When you download the configuration package and install it then is the manual directly on your PC, look in the SIMATIC/Documentation directory. [:o] A update of the hardware catalog over a Hardware Support Package can be done when you are online and in the "HW Config" -->"Options" --> "Install HW Updates ...". Here you can choose between "Download from the Internet" and "Copy from disk", when you have the possibility to be online then only chose "Execute...". The first time you have to give up a directory where you want to install the HSP. When you don't have the possibility to get directly on internet with your programming device, then you can download the Hardware Support Packages (HSPs) under the next link: http://support.automation.siemens.com/WW/view/en/23183356 For installing i refer to the part above..... [;)] |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on