12/2/2022 10:20 AM | |
Joined: 12/2/2022 Last visit: 6/7/2024 Posts: 1 Rating: (0) |
hello, I have multiple button on hmi screen. which are used for object selection, when I am going to press any button at HMI screen then I/O field at HMI screen shows object information and tags give the command to plc to fetch the information from SQL database and print it through printer. problem is that, when I am select any object than this selected object not stable at HMI randomly alter by zero. change by zero only and reappear. due to this, fetched information from SQL database is also become zero randomly. and printer also print zero as per previous process. i have multiple network where these selected object is reseted to eliminate the multiple selection of objects so how can i fix it ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/02/2022 11:56:22New subject after splitting |
|
Follow us on