4/12/2023 6:08 AM | |
Joined: 2/18/2020 Last visit: 4/27/2024 Posts: 1 Rating: (0) |
Hello, please help, the controller has gone to stop Diagnostic buffer of module CPU 317F-2 PN/DP Order No./ Description Component Version 6ES7 317-2FK14-0AB0 Hardware 5 - - - Firmware V 3.2.10 Boot Loader Firmware expansion A 37.11.12 Rack: 0 Slot: 2 Serial number: S C-DDUW62792013 Event 1 of 500: Event ID 16# 457F STOP caused by STOP command FB number: 1639 Module address: 3084 Previous operating mode: RUN Requested operating mode: STOP (internal) Internal error, Incoming event 11:21:17.269 AM 04/12/2023 (Coding: 16# 457F FF84 8E00 0C23 0667 0C0C) Event 2 of 500: Event ID 16# 75D1 Safety program: internal CPU error Internal error information: 7:0000 Instance DB no. of the causing F system block: 1638 Previous mode: RUN Requested mode: STOP Internal error, Incoming event 11:21:17.265 AM 04/12/2023 (Coding: 16# 75D1 9F84 C47A 0666 0007 0000) Event 3 of 500: Event ID 16# 4302 Mode transition from STARTUP to RUN Startup information: - Startup with modified system configuration - Difference between setpoint and actual configuration - Time for time stamp at the last backed up power on - Single processor operation Current/last startup type: - Warm restart triggered by switch setting; last power on backed up Permissibility of certain startup types: - Manual warm restart permitted - Automatic warm restart permitted Last valid operation or setting of automatic startup type at power on: - Warm restart triggered by switch setting; last power on backed up Previous operating mode: STARTUP (warm restart) Requested operating mode: RUN Incoming event 11:21:17.156 AM 04/12/2023 (Coding: 16# 4302 FF68 C700 0000 0B13 7713) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/12/2023 10:38:59New subject after splitting |
|
4/12/2023 10:57 AM | |
Joined: 7/19/2022 Last visit: 5/14/2024 Posts: 358 Rating: (61) |
Hello VladimirSnoochi, I recommend that you take a look at the following FAQ: |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on