12/28/2023 8:49 AM | |
Joined: 6/6/2023 Last visit: 1/31/2024 Posts: 1 Rating: (0) |
While operating CPU went to STOP mode and all leds were flashing. I restart CPU by switching power off and on and looked at diagnostic buffer. The first message in buffer is: Event 64 of 64: Event ID 16# 4580 STOP: backup buffer contents inconsistent (no transition to RUN) Previous operating mode: No voltage Requested operating mode: STOP (own initialization) Internal error, Incoming event 00:00:00.000 1994-01-01 From what i understand CPU checked data on backup buffer, found inconsistency and put CPU in STOP mode. My question is when the CPU checks backup buffer for consistency? Only when power on or during operation too? Attachment27_12_2023.txt (235 Downloads) |
1/4/2024 8:01 AM | |
Joined: 3/11/2019 Last visit: 5/6/2024 Posts: 1397 Rating: (248) |
Hi, for event id 16# 4580 there was an improvement made with firmware V3.2.7, in the meantime firmware V3.2.19 is available. Firmware updates for CPU 319F-3 PN/DP (6ES7318-3FL01-0AB0Firmware update V3.2.7 provides the following corrections:
regards sancruz |
Feedback appreciated, please rate |
|
Follow us on