Industry Online Support
Technical Forum
7/27/2009 8:56 PM | |
Joined: 10/8/2008 Last visit: 5/17/2024 Posts: 43 Rating: (0) |
Hello, We tried to build an communication between a PLC 315 PN as a slave and the masster which is a device M232 from Foxboro. We can see that the bit for the established connection is on but we can not see dataflow, the bits busy and done stay at zero. For this project we used the software and wizard version 2, is it possible that we need the new software Fb102 version 3.1 instead off version 3.0. Also we had problems what to do with the port numbers 502 and 2000. Can someone advice us what is wrong in this programm Thank in advance Jan AttachmentModbus_p.zip (587 Downloads) |
7/28/2009 7:51 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already discussed in the thread with the subject Communication between PLC and master Invensys (module M232) . You can find it within the conference OpenModbusTCP Best regards O_Moderator |
Follow us on