Industry Online Support
Technical Forum
7/17/2009 11:12 PM | |
Posts: 10 Rating: (0) |
Well, my first tests with Modbus TCP were also only 2 Stations, and it worked very well and fast. In my current configuration, i have 45 Stations, resulting in a communication cyycle time of about 1 second between one reading cycle and the next. So probably my problems may be caused of the count of stations? But however - when i'm in the A083 state, the ERROR is TRUE - so what else do i have to wait for? Since i did the hack, it works like a charm. I decided to attach the SCL Source File. I hope, i explained most of the code in my first posts :-) Greets Hans AttachmentMODBUS_TCP.zip (510 Downloads) |
Follow us on