9/27/2009 3:18 AM | |
Joined: 10/7/2005 Last visit: 10/19/2024 Posts: 3024 Rating: (1054) |
Hello Tomy Master Catalogue ST70 has this info as well as the "CPU Technical Specification manual" (seelinksbelow): SIMATIC S7-300 CPU 31xC and CPU 31x: Technical specifications SIMATIC S7-400 S7-400 Automation System, CPU Specifications P.S: You may also find Aret's answer in thethread"DB Size" useful. I hope this helps. |
Cheers |
|
9/30/2009 3:17 PM | |
Joined: 2/6/2009 Last visit: 8/19/2024 Posts: 939 Rating: (118) |
HI, It is very simple to get the details about the address areas supported (including the DB's) by a PLC. Just open your program -> go online with PLC or Simulator -> Right click the station (SIMATIC 300) -> goto PLC -> Module Diagnostics (or press CNTRL+D). Select the perfomance data menu for the New Module information Window and you can get the details about the OB, DB, M,FB,FC everything.Use the print option to get the detail spec of that CPU. The above point are given as print screens in the below attachment. Attachmentdata's.zip (267 Downloads) |
_______________________________________________________________ |
|
This contribution was helpful to1 thankful Users |
Follow us on