Industry Online Support
Technical Forum
6/21/2010 5:04 PM | |
Joined: 9/27/2006 Last visit: 5/26/2024 Posts: 12257 Rating: (2668)
|
Hello Usman; Have a look at SSD Parker drives information pages, to begin your research: SSD Parker supported communication protocols: http://www.ssddrives.com/usa/Products/Communications.php SSD resource center-Communications: http://www.ssddrives.com/usa/doc/Communications.php -Profibus Tips -L5353 S7 Profibus setup As you can see, your question is reversed. Since Profibus-DP is supported by SSD drives, you must confirm if the model you have selected supports it (this is not at all certain, it will depend on the manufacturer).Once you have confirmed it, any Siemens S7-300 CPU that has an integrated Profibus-DP master interface (CPU 31x-2DP), or which has an attached CP 342-5 DP-master comm.. processor will be able to talk to the drive.There is an application note showing how a L5353 drive can be connected to a Siemens PLC using Profibus, use it to base your own application. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/21/2010 5:06 PMLast edited by: dchartier at: 6/21/2010 5:05 PM |
|
6/22/2010 6:06 AM | |
Joined: 6/10/2010 Last visit: 11/20/2022 Posts: 12 Rating: (0) |
Boundle of Thanks The given information is really helpfull. |
Follow us on