6/10/2010 8:44 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Hello melsec-, You'll continue to fight with old,old Siemens staff. Good luck! Best regards, Hristo Mihalev |
6/10/2010 9:53 AM | |
Joined: 11/21/2007 Last visit: 6/24/2024 Posts: 2324 Rating:
|
Dear UMENCHO You are right, it is not possible to go ONLINE to S5 110A using PC-675 as it does not have a Parallel communication interface. Pl see theS5 110A manual Below : http://support.automation.siemens.com/WW/view/en/21190174 However I have ( Long Long Time back ) used a PG 675 and Read / Blown the S5 110A EPROMsin offline mode without any problems. @melsec .. Oops ... it was " P0 " STEP5 software and not SA ... SB.. that was used in PG-675 forS5-110S ( Looks like my memory was notso good on this ) . See the FAQ Below : http://support.automation.siemens.com/WW/view/en/188158 This confirms that you can read 110A EPROMS on PG675 but with only P0 version of the STEP5 software. @melsec - this also confirms your worst fears -- what you have is a S0 version , which does not support S5 110A / 130A / 130K . Only choice is to get hold of a P0 disk ( If anyone has any !! ). We used to have a disk lying around until a few years ago .. however we dumped it after our PG-675 failed beyond repairs. Cheers Navnag |
Last edited by: Navnag at: 6/10/2010 9:55 AMThere is no such thing as the last bug in a program |
|
This contribution was helpful to
1 thankful Users |
Follow us on