Industry Online Support
Technical Forum
9/23/2010 10:09 AM | |
Posts: 42 Rating: (1) |
Please check the attachment.For reading data from FM-350-1 via PROFIBUS ,is it posible to use FB127(CH_CNT,PCS7) in a non PCS7 project.Please check the other picture for a proximity sensor which generate 24-volt pulse train according to the machine speed.Can I use the module to measure the speed of the machine with this function? AttachmentFM350-1.zip (119 Downloads) |
Last edited by: ROCLIM at: 9/23/2010 10:12 AM |
|
9/23/2010 7:48 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello, Blocs written for PCS7 in many cases include specific channel drivers. For a standard project, there is another libary. The configuartion software package includes samples with the needed FCs to be used. The software can be found here: http://support.automation.siemens.com/WW/view/en/28291262 Here the manual. http://support.automation.siemens.com/WW/view/en/1086726 |
Best regards |
|
Follow us on