12/13/2010 7:40 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Hello, in attachment you can find the files sent to me by fly. Best regards O_Moderator Attachmentattach.zip (93 Downloads) |
12/29/2010 2:09 PM | |
Joined: 10/7/2005 Last visit: 9/5/2024 Posts: 3018 Rating:
|
Hello fly before we get to your question, allow me to ask you if you are aware that this is a forum and not the Siemens Technical support hotline? People contribute here on their own free will to help each other and to share knowledge and I would thank jklmfor extendinghishelp to you if I were you. Now that we got that out of the way, let's see if I'm the "serious guy" who can help you. To start with, if would have helped if you would have given a bit more info about your problem. Iwill however make an educated guess andassume thatthe troubled FC88 callof the STL source filefrom your original post is the converted call of FB204(called from FB133) of your original S5 program, correct? If so, it is a 32 bit division block (aptly called "DIV:32" in the S5) and may be replaced byFC88 from "S5-S7 converting Blocks" library. Alternatively (this is what I would do)throw it away and simply use the inbuilt Double Integer division (together with modulo if required) instead. By the way, the reason for the error in your source file compilation (ref thepicture of yoru original post) is simply because you use a BYTE (DBB104) instead of a WORD (e.g. DBW104) for the Z_12 parameter of FC88 (note that your S5 program has quite correctly DW52 assigned to this paramater which the converter would have converted to DBW104, did you edit the source file?). Anyway,not such a "strong debug" after all and I hope this helps |
Last edited by: fritz at: 12/29/2010 2:18 PMCheers |
|
This contribution was helpful to
2 thankful Users |
1/11/2011 4:15 AM | |
Posts: 11 Rating:
|
Thanks for you help, thisresponse are reallyserious,forgive to me, my lastcomment, but you know, that was to call theattentionbecause some time, the respondsdoesn'tenough. and I didn't know that the forum was a freevolunteersupport. Thank you very much, foryourhelp again!! your aseriousguy!!! Her fritz !!!! And Please, I have another question for you, if I have aS5CP 524 poin to point, I need to select a CP in S7 400, but I needto know the S5 CP 524 configuration parameters, over all the inputsassignment, can you help to me whatsoftware in S5 I need?? to select the correct S7 400 CP....see the attachment file Best Regards my friend!!! |
1/11/2011 5:44 AM | |
Joined: 10/7/2005 Last visit: 9/5/2024 Posts: 3018 Rating:
|
Hello fly you'll need COM525 and can find the manual for it HERE(part 1/2, it also includes the CP524 description)and HERE (part 2/2). Having said that, your picture does NOT show aSiemens CP524 but instead aWestinghouse made version of it which may - or may not - be functionally identical to the one described in the Siemens manual. I hope this helps |
Cheers |
|
1/11/2011 6:37 AM | |
Posts: 11 Rating:
|
hello fritz: you are the guy, can you send to me your personal email, this is my willard.garcia you know in gmail. Best regards
|
Follow us on