12/7/2006 11:56 AM | |
Joined: 4/24/2006 Last visit: 11/6/2024 Posts: 8768 Rating: (1170) |
Hi alexfizeau, Did you install Protool Pro RT also? Or only Protool Pro CS. Best regards, Wizard |
12/7/2006 1:39 PM | |
Posts: 95 Rating: (0) |
Yes, ProTool CS, ProTool Runtime, ProTool Loader and ProTool Simulator are installed. And only ProTool Runtime cannot be used... |
12/7/2006 1:48 PM | |
Joined: 4/24/2006 Last visit: 11/6/2024 Posts: 8768 Rating: (1170) |
Hi, Which type of panel are you programming? Best regards, Wizard |
12/7/2006 1:49 PM | |
Joined: 5/8/2006 Last visit: 10/16/2024 Posts: 1085 Rating: (77) |
Hi, sorry, I read over.Is the file PTProRun.ini in the ProTool path available? Bye |
12/7/2006 8:13 PM | |
Posts: 95 Rating: (0) |
So that's the reason. Many thanks. |
Follow us on