8/3/2011 7:00 PM | |
Joined: 9/19/2009 Last visit: 9/10/2024 Posts: 459 Rating: (85) |
Hi Everybody! I would like to know why I can´t change the CPU in Hardware configuration. I have a old project and I want to change the CPU 317 for the new CPU 319. I´m going to hardware configuration and then I try to do it, but this one not appears. There is an attachment picture. I know that I can delete the old CPU and then insert the new and load all the modules, OB,FC,FB... It's just curiosity. Thanks advanced. |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
8/3/2011 11:25 PM | |
Joined: 9/19/2009 Last visit: 9/10/2024 Posts: 459 Rating: (85) |
What is the order number (MLFB) of the New CPU you want to use and also the version of STEP7 you are using? Check if the new CPU can be programmed by current version of STEP7 . To do the changes, make a copy of the old project.Modify the hardware (Keep the old settings for CPU and network) and then compile it (you may loose the blocks here).Copy the blcoks from original project the revised version. Hope to be helpful. Regards Thank you very much!!! The number of the CPU-319 (6ES7 318-3EL01-0AB0) and the version of Step7 5.5. I can see this CPU in my Hardware and I can create a new program with that, the problem was when I trying of change the CPU in an old project. To do the changes, make a copy of the old project.Modify the hardware (Keep the old settings for CPU and network) and then compile it (you may loose the blocks here).Copy the blcoks from original project the revised version. That is right!!! works perfectly, the cuestion was because I can´t change it. Thanks you! Best Regards |
Last edited by: JM76 at: 8/3/2011 11:26 PMIf my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
8/4/2011 2:47 PM | |
Joined: 9/19/2009 Last visit: 9/10/2024 Posts: 459 Rating: (85) |
Thanks you very much! Best Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
This contribution was helpful to1 thankful Users |
Follow us on