2/1/2012 9:16 AM | |
Posts: 140 Rating: (0) |
Hello Experts, I am facing an issue that MY PLC’s (315T-2DP CPU) SF LED is continuously blinking and I can’t even establish a connection with my PLC to download any program into it. I have attached the project that I am using. Please suggest the solution asap. Is it a hardware problem? It was working fine until I reset it using the attached procedure. Thanks! Attachments7300 cpu 31xc and cpu 31x operating instructions en US en US 1 pdf.pdf (182 Downloads) |
2/1/2012 11:18 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already published in the following thread SF LED Continuously Blinking Problem Best regards O_Moderator |
Follow us on