Industry Online Support
Technical Forum
4/17/2009 1:37 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello arturas, Basicly in path name field should be AS511-MUX-ENDP. Try to select this. Double click there and look at C:\Step5\S5_SYS\AP_INI.... The other possible things are: You had to use com 1 with settings: 9600, 8, N, 1, N. ... More settings look at "System message no. 0334" when attempting to go online with STEP 5 V7.2 in Windows XP Hope this will helps. Best regards Hristo Mihalev |
2/20/2012 1:23 PM | |
Posts: 3 Rating: (0) |
Try using PG2000 instead. Easier to use then dos based program. |
Follow us on