2/27/2012 10:35 AM | |
Posts: 20 Rating: (1) |
Question: I downloaded the websever example that was posted above. Entered the project (i changed the cpu to 1212C ac/dc/rly v2.1), enabled the webserver, linked the html-page en generated the blocks. Compiled the program with no problems. Than I started the downloadpocess, it compiles again without problems but when i click load there are some warnigs, the infotab says that there are some problems with the included jquery files and will be ignored... I had some other projects with jquery files and had the same problems.. What could be wrong or has to be changed??? Some help would be realy great! Thanks in advance |
Last edited by: O_Moderator at: 2/27/2012 11:58 AMnew subject after splitting from /tf/WW/en/Posts/66290#top |
|
2/28/2012 1:39 PM | |
Posts: 20 Rating: (1) |
Asked for support.. i will post the anwser here. @huggy, why would someone create an example project with jquery when it doesn't work? |
2/29/2012 7:58 AM | |
Posts: 20 Rating: (1) |
Could be, the software i'm using is v11 sp2, and plc is 1212C ac/dc/rly v2.1. The example program is a 1214C dc/dc/dc v2.1 So it should be the same, right? |
Follow us on