Industry Online Support
Technical Forum
6/19/2012 9:44 AM | |
Posts: 18 Rating: (0) |
hi dear ihave a module 6fm1726-3ca00 i want tochange it to s7. I don't know which module should i replace it. |
6/19/2012 4:37 PM | |
Joined: 9/27/2006 Last visit: 5/27/2024 Posts: 12257 Rating: (2668) |
Hello sarana; The part number you posted refers to a S5 positionning module for absolute encoders, WF 726C. One option in the S7-300 family is SM 338: http://support.automation.siemens.com/WW/view/en/14411783 Supported encoder types Encoder types supported by SM 338; POS-INPUT: ● Absolute value encoder (SSI), frame length 13 bit ● Absolute value encoder (SSI), frame length 21 bit ● Absolute value encoder (SSI), frame length 25 bit Supported data formats SM 338; POS-INPUT supports gray code and binary code. Another option is to look for absolute encoders with a Profibus-DP connection, that you could simply read in through the integrated DP port of the CPU. A few examples: User Manual Absolute value encoder with PROFIBUS-DP Absolute Encoders Profibus DP PROFIBUS Encoders - Absolute Rotary Encoders For Industry CE-65-M PROFIBUS-DP Encoder Hope thie helps, Daniel Chartier |
Last edited by: dchartier at: 6/19/2012 4:38 PM |
|
This contribution was helpful to1 thankful Users |
6/20/2012 11:44 AM | |
Posts: 18 Rating: (0) |
thanks a lot it was so useful
|
Follow us on