5/26/2007 10:39 AM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
Hi Sulung, You program the two IM153-2BA01 behind two different CPUs and will see them together in Netpro. Only in the hardware configuration of the H-System you will see the two IMs together. Do you have two CPU 319 PN/DP ? So it is only cheaper to buy a redundancybundle, the part is not in the hardwareconfiguration. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
5/29/2007 9:53 AM | |
Joined: 5/26/2007 Last visit: 5/9/2024 Posts: 127 Rating: (3) |
Dear Late, Thanks alot for your tips. I got it now. best regards, sulung |
5/29/2007 5:11 PM | ||
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1425) |
Hi, just to remember, if you make a configuration with 2 CPU S7-300 in software redundancy mode, you need to install de software redundancy package first. |
|
Denilson Pegaia |
||
5/31/2007 9:03 AM | |
Joined: 5/26/2007 Last visit: 5/9/2024 Posts: 127 Rating: (3) |
Hi, do i have to order a separte software redundancy package? or is it available for download? Something very strange is going on and i do not know what. when i said i got it, i program two IM153-2BA01 behind two different CPUs and i see them together in Netpro. but i could only build one node (see graphic3.jpg). Then i make a new project trying the trick again, but this time i could not use this "insert redundancy" under edit menu. please see my attachment, graphic1.jpg and graphic2.jpg. please help me. thanks alot. |
5/31/2007 5:08 PM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1425) |
Hi, sorry, but you need to but the software. See ST70 chapter 7 (www.siemens.com/simatic/printmateria). |
Denilson Pegaia |
|
6/3/2007 3:02 AM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
Hi, The "insert redundancy" is only for the H-System. You must define the CPU 315 PN/DP seperately and only place the slaves after that in Netpro to each other so that you are knowing that they belong together.... |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
6/4/2007 6:47 AM | |
Joined: 5/26/2007 Last visit: 5/9/2024 Posts: 127 Rating: (3) |
THANK YOU EVERYBODY!! finally i get it. just missed some step. thanks again. |
Follow us on