Industry Online Support
Technical Forum
6/19/2007 2:05 PM | |
Joined: 11/30/2006 Last visit: 5/10/2024 Posts: 59 Rating: (0) |
Hello to all, I am trying to put some of the Process Value Archives in totheCSV file. Finally I stucked with Industrial Data Bridge v6.1 SP1. I tried to use WinCC OLEDB to CSV option and manadged to establish connection but my CSV file was empty all the time. I assumed that I did not configure things well I opened Industrial Data Bridge demo project to see what I did wrong. I was supprised when I saw that when I try to do the connection in Runtime it is not possible. In the attachment you have pictures of Runtime and Trace View. I use WinCC v6.0 SP4. Please can you explain me what is wrong. AttachmentIDB.zip (233 Downloads) |
Follow us on