Industry Online Support
Technical Forum
5/16/2013 10:13 AM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating:
|
Hello, which type of S5 and S7? 6ES5 ... / 6ES7... Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de
work faster withinnovative PLC-Tools |
5/16/2013 12:03 PM | |
Posts: 119 Rating:
|
S5 6ES7 "110U" S7 6ES7 "314 2DP" |
5/17/2013 7:18 AM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating:
|
Hello, please the complete order no. 110U?? 101U or 115U? Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de
work faster withinnovative PLC-Tools |
5/17/2013 8:11 AM | |
Posts: 119 Rating:
|
Actually it was 100u order number 6es5 998 0ub22 ,but is that info relevent ???? Please tell me how to use switch between I/O's of both PLC's |
5/17/2013 9:23 AM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating:
|
Hello, yes i need this information. The order-no is with included documentation (old order-no). The CPU must be a 6ES5 100-8MA02.You can disconnect the CPU from the IO-modulesand use a 6ES5 318-8MB12 / 13 to connect the S7 with the IO-modulesvia Profibus. Then you can very fast change the CPU S5 <--> S7. Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de
work faster withinnovative PLC-Tools |
Follow us on