Industry Online Support
Technical Forum
11/10/2005 1:09 PM | |
Posts: 3149 Rating: (171) |
Hello Demi, well, how do you want to generate your Alarm => e.g. with ALARM8 blocks in the CPU? or do you just want to use a bit in e.g. in DataBlock, which is transfered by AS/OS-Engineering to a Variable, which is triggering an Alarm? =>then you can use e.g. in Alarm loggin a Single Message , where you can assign a Bit of a WinCC variable. http://support.automation.siemens.com/WW/view/en/22062395 Good luck, Nemo |
11/11/2005 12:46 PM | |
Joined: 9/1/2005 Last visit: 5/14/2024 Posts: 4101 Rating: (194) |
Closed: cause topic posted twice. Here you will find the second topic with the reply: DB-Addressing |
My Forum is the place to personalize your profile, |
|
Follow us on