7/11/2013 6:56 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Thanks Kaulquappe I think, I will try to explore the option of using a IM151-8 for each section and then transfer the data from IM151-8 to S7-400H. Any idea what is the limit of PAC3200 meters on IM151-8 if I use Modbus TCP/IP or Profinet ? Presently I had considered the PAC3200 connected on Profibus and we were planning to read 2-3 important parameters on DPV0 while remaining parameters on DPV1. However as per the comments I received on my Post ( /tf/WW/en/Posts/93972#top) DPV1 is not possible downstream of a Y-Link module for PAC meters. This would result in using a very large no of Y-Links as I cannot connect more than 5-6 meters on one Y-Link. Thanks Navnag |
Last edited by: Navnag at: 7/11/2013 7:06 AMThere is no such thing as the last bug in a program |
|
Follow us on