Industry Online Support
Technical Forum
3/24/2014 11:11 PM | |
Joined: 7/27/2012 Last visit: 9/12/2024 Posts: 1 Rating: (0) |
Hi, I have a feeder that use feedback of material position a measure wheel. The feeder work well but if I lock the measure wheel the "DAC" go to 10V but without any error . How I can have a alarm indication in this situation ? Can I have a alarm when a follow error is more than a fix value ? On attachment the feeder DM Best Regards Mauro AttachmentOFFLINE.zip (89 Downloads) |
Follow us on