Industry Online Support
Technical Forum
11/19/2014 1:06 PM | |
Joined: 6/26/2013 Last visit: 4/23/2024 Posts: 143 Rating:
|
Dear All, Inan S595U system, S5 code contains five PID calls. The block used is FB203 (I-REGLER = Impulse Controller) for a heating process. I am using FB41 (CONT_C) + FB43 (PULSEGEN) in the converted S7 code because in S5, both heating and cooling were done simultaneously (that is why I am not using FB58 (TCONT_CP) because it can only do one thing at a time - heat or cool). So now I need help in parameterizing FB41+FB43 in S7 code. I have read some relevant FAQs. Kindly find attached pdf file containing all S5 PID calls and parameters. Regards. AttachmentPID_CALLS_&_SETTINGS_IN_S5_CODE_VACUUM_PYROLYSIS.pdf (305 Downloads) |
Last edited by: Min_Moderator at: 11/19/2014 1:42 PMEdit attachment name Last edited by: meeda at: 11/19/2014 1:08 PMLast edited by: meeda at: 11/19/2014 1:07 PMmeeda_ |
|
Follow us on