1/25/2015 8:17 AM | |
Posts: 7 Rating: (0) |
Hello Dear Sir; many i know what is the main differences between following two modules of CPUs S7-1200 series? 6ES7214-1HG31-0XB0 & 6ES7214-1HG40-0XB0 Best Regards! Seyedi
------------ New subject after splitting from what is the main differences between 7kf02 and 1kf01. |
Last edited by: Min_Moderator at: 1/26/2015 9:46 AMSplitted |
|
1/26/2015 11:19 AM | |
Joined: 5/29/2013 Last visit: 10/14/2024 Posts: 100 Rating: (28) |
Hi SMSSSB, The 31 and 40 stands for the factory default Firmware of the CPU. Where V3x and V4x stands for hardware changes (so you really need the new CPU for the update) Vx1 and Vx0 stands for updates in the same Hardware CPU. A firmware upgrade of the S7-1200 CPU modules is possible only from V.1x to V2.x. It is not possible to make a firmware upgrade from V2.x to V3.x nor from V3.x to V4.x. The firmware V2, V3 and V4 each require corresponding CPU hardware. Where you could use V31 and lower in Tia Portal V12 You need Tia Portal V13 for V40 and Tia portal V13 SP1 for V41. See attached links to see the updates on V4.0 Sales/Delivery Release: S7-1200 CPU V4.0, CPU 1217C and IO-Link Master SM 1278. Note: V41 is last month released and will be available as factory default in the coming days. Firmware Version V4.1 released for S7-1200 CPUs If your planning to use it than you also need to update your Tia Portal V13 to SP1 Service Pack 1 for SIMATIC STEP 7 V13 incl. PLCSIM (TIA Portal) |
Regards |
|
This contribution was helpful to1 thankful Users |
Follow us on