2/8/2015 11:07 AM | |
Posts: 5 Rating:
|
dear all, have a good day: i am mahmoud, from Egypt, i have a problem with S5 95U that i cannot access to the analog input on the CPU,the onboard i/os, i have just graduated from the faculty, and i'm new in this matter. i have written my program using PG 2000, i added new OB1 and i wrote my program in it directly calling FB250 which is the function used for the analog inputs, and i have constructed a DB1 to get the value of the input analog in it. as regard the H/W, i have a PT100 sensor and a converter which is used to convert the resistance o/p in 0-10v signal. i have taken a screenshots for my program to make it easy to understand. please help me to solve this problem i'm wating your reply as soon as possible ---------------- Attachments5.docx (127 Downloads) |
Last edited by: Min_Moderator at: 2/9/2015 9:38:11 AMNew subject after splitting |
|
2/8/2015 12:17 PM | |
Joined: 12/18/2014 Last visit: 6/17/2024 Posts: 33203 Rating:
|
You use in your program DB1 for data storage. This is not good because the DB1 is used for internal purposes. You must also released the analog input for reading in DB1. Here you can download the manual for the S5-95Us. Attachments5_2.docx (116 Downloads) |
This contribution was helpful to
1 thankful Users |
2/8/2015 1:32 PM | |
Posts: 5 Rating:
|
i am sorry but my problem still exists, the attachment shows my changes Attachments5.docx (92 Downloads) |
2/8/2015 3:31 PM | |
Joined: 12/18/2014 Last visit: 6/17/2024 Posts: 33203 Rating:
|
Sorry, I've forgot the link for the manual. https://support.industry.siemens.com/cs/attachments/1091648/6ES5_998-8MA22.pdf |
Last edited by: Min_Moderator at: 2/9/2015 9:42:23 AMChange link to permanent |
|
2/8/2015 3:47 PM | |
Posts: 5 Rating:
|
i have already seen the manual,but i think my problem is related to the software not to the hardware i am using pg2000 v4,65 . |
2/9/2015 12:46 PM | |
Posts: 5 Rating:
|
dear experts; i am facing a a problem, can anybody help me ? |
3/10/2015 10:17 PM | |
Posts: 2661 Rating:
|
Hi rimoon, See section 12.1 in the manual - "Specify in DB1 which analog inputs are to be read into the PII cyclically" Regards |
Follow us on