1/27/2015 2:38 PM | |
Joined: 1/21/2013 Last visit: 10/23/2024 Posts: 4620 Rating: (708) |
Hello, You can only use the OB1 as long as you do not make mistakes such as programming, then you can call the OB121, be careful to use this organization blocks because if you have a problem your CPU does not change to STOP "remains in RUN" can cause problems !!!! You can use OB100 which is the organization block initialization if you have such reset or set of flags before the start of OB1. Read the first chapter below that are all the organization blocks, be careful that in your CPU 315-1AF03 will not have all these OBs. Reference Manual for S7-300/400 System and Standard Functions Wrote: Which OBs Are Available? Not all CPUs can process all of the OBs available in STEP 7. Refer to Operations lists /72/ and /102/ to determine which OBs are included with your CPU. |
Last edited by: Ste39 at: 1/27/2015 2:56 PMLast edited by: Ste39 at: 1/27/2015 2:41 PM |
|
6/7/2015 7:18 AM | |
Joined: 9/1/2005 Last visit: 11/8/2024 Posts: 4111 Rating: (195) |
new question published by DungNBQ is split to a seperate thread with the subject S5 100U TO S7 300: corresponding module and function code
Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on