5/2/2008 4:05 AM | |
Posts: 15 Rating: (0) |
Hi! On the screen of "SIMATIC Manager" Is it the screen displayed by "View-->Online"? The appended PDF file is seen. FC82 was not shown in the screen displayed by "Online." Isn't there any FC82 into CPU? To a trial The place which copied FC82 to the screen of "Online" from the screen of "Offlin", It will be displayed as "Uneable to copy the block FC82." If it carries out what Can FC82 be put into CPU? Please teach me......Thanks Attachmentmelsec1.pdf (335 Downloads) |
5/2/2008 5:50 AM | |
Joined: 9/27/2006 Last visit: 5/1/2024 Posts: 12257 Rating: (2666) |
Hello melsec; I have found the answer to your problem on Siemens support FAQs; http://support.automation.siemens.com/WW/view/en/18257607 QUESTION: Why can't block from the standard library "S5-S7 Converting Blocks" be loaded into a CPU 312C? Now you are allowed to use crying symbols: Your tests will need a different CPU, even a CPU313C will work. Hope this helps, and sorry I have no better answer for you (even though you did learn a thig or two about diagnostics on these CPUs) Daniel Chartier |
Follow us on