Industry Online Support
Technical Forum
5/1/2008 11:54 AM | |
Posts: 9 Rating: (0) |
I have a PG P4 that the cpu usage goes to 100%, then slows to a crawl and eventualy locks up. Does anyone have any thoughts on what can be done to correct this? |
5/2/2008 8:30 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (316) |
Hi, Which software do you have installed ? It could be that a "over"-installation of several STEP7 versions give some problems. Have you checked on viruses.... If non of the above are tipycal for you, then you might deinstall the Software completely, see the FAQ: How can you completely uninstall STEP 7 including all the software packages? If there is after installation of STEP7 V5.4 SP3.1 direct trouble again, then please install the total recovery...... |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on