6/15/2017 10:01 AM | |
Joined: 6/22/2015 Last visit: 5/7/2024 Posts: 2 Rating: (0) |
Dear sir I have Smart 200 PLC with 4 Encoders of A phase (Single channel). I have issue that if I connect the one Encoder to I0.0 and other is to I0.1, If I start the first motor (encoder connect with I0.0) then I am getting pulses to Both I0.0 and I0.1. If I connect only one Encoder to I0.0 then its working OK. Same thing happen with I0.2 & I0.3. Please give me solution. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/19/2017 5:38:50 PMNew subject after splitting |
|
Follow us on