9/12/2017 11:13 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi, 6ES7322-1HH01 is the succesor of the 1HH00. It is full compatible. So the wiring is the same like the predecessor. by using the search bar in the upper right it is easy to find this information. It is a relay-output-module. the pin 10 needs 24 VDC, pin 20 needs 0VDC. Pin 1 and pin 11 are giving the potential you want to switch with the relay-outputs. It can be 48V - 120V AC or 24V - 120V DC. unfortunally the technical data are only available in german. the succesor can handle a higher voltage. SM322 Digital Output Module With 16xRelay 120/230V: New Version Now Available hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
9/12/2017 11:46 AM | |
Posts: 42 Rating: (0) |
Thank you sir mopSO4, sir patriot.m aur jacked f for your precious suggestions |
Follow us on