12/7/2017 7:50 PM | |
Joined: 2/5/2015 Last visit: 9/27/2023 Posts: 127 Rating: (0) |
Hello guys, My software version in TIA PORTAL V14. The CPU I´m using is s71200 DCDCDC fw3.00.02. When I try to download my project I get the message "incompatible device". The IPs are in the same range. In the window "select target device" I can see the CLP and the IP 192.168.0.1 but it´s not possible to download because it says "incompatible device". My PC has the IP 192.168.0.10. What could be wrong!? Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/8/2017 8:34:30 AMNew subject after splitting |
|
12/8/2017 1:16 PM | |
Joined: 4/24/2006 Last visit: 5/23/2024 Posts: 8657 Rating: (1154) |
Hello, Here is a faq: Or use the SIMATIC Automation Tool: SIMATIC Automation Tool - the commissioning and service operation tool for SIMATIC modules Best regards, Wizard |
This contribution was helpful to1 thankful Users |
Follow us on