12/7/2017 10:21 AM | |
Joined: 11/27/2015 Last visit: 5/28/2024 Posts: 7 Rating: (0) |
A question regarding the actual length. When or how is the byte [1] "Actual lenght" updated? if the string is a dynamic string updated with FC31 "replace" i would expect the actual length to be updated?. So my question is, wich options do i have to update header information "actual lenght"? This is a issue when using keepware OPC keepserver, is the serover only reads the number og charaters thats numberes in actual lenght. /Kasper. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/7/2017 2:09:23 PMNew subject after splitting |
|
12/9/2017 9:43 AM | |
Posts: 8946 Rating: (999) |
Yes. |
Follow us on