6/4/2016 8:19 PM | |
Posts: 3 Rating: (1) |
Sry for the long time... sure, just try to try to generate the db´s for the webserve with that file. you have to change the .txt to .js i could not upload a file with .js extension. if you try to generate the db´s for your webserver you will only get the status: inconsistent thanks a lot Attachmentjquery-2.1.4.min.txt (158 Downloads) |
9/15/2017 8:24 AM | |
Joined: 6/1/2012 Last visit: 12/6/2019 Posts: 1 Rating: (0) |
digite da seguinte forma que funciona for (var i = 0; i < data.length; ++i) { res.push ([[i], data[i] ] ) |
1/31/2018 8:18 AM | |
Joined: 10/2/2014 Last visit: 8/5/2024 Posts: 88 Rating: (15) |
pls. see also the App Example - extent examples - on the support websides: Creating and using user-defined web pages on S7-1200 / S7-1500 They are using AJAX request from jQuery and JSON as format to transfer the data. Regards |
Follow us on