3/28/2018 11:22 AM | |
Posts: 171 Rating: (44) |
Once I did changing the tags of the "Online Trend control" in WinCC 7.3 using scripts. But I dont know how to do this in V14. |
3/28/2018 12:30 PM | |
Joined: 1/5/2013 Last visit: 5/24/2024 Posts: 275 Rating: (16) |
I think the same, do you mean option3? |
3/28/2018 12:58 PM | |
Posts: 171 Rating: (44) |
Yes. Change .txt to .pdl Check this one with WinCC 7.3 or 7.4 I dont have Wincc v14 prof since i've wincc 7.4. otherwise i'll check that too. In this I did script to change the tag in runtime. Try like this in V14 Attachmentword.txt (69 Downloads) |
3/28/2018 2:19 PM | |
Joined: 1/5/2013 Last visit: 5/24/2024 Posts: 275 Rating: (16) |
thank you, but I can't open the file with .pdl, can you save the code with pdf format? |
3/28/2018 3:00 PM | |
Posts: 171 Rating: (44) |
Is this ok?
|
3/29/2018 3:40 PM | |
Posts: 171 Rating: (44) |
I think the possible way is to use tagprefix method only. |
Follow us on