7/11/2019 1:16 AM | |
Posts: 1 Rating: (0) |
Hi, I have tested with the nodes and it only works with the USER button. I have installed the Input / Output module but I do not identify the digital inputs D0-D13. I need to connect two buttons and I do not know how to connect them. Attached photo of the module. Need help please ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/11/2019 13:06:07New subject after splitting |
|
7/11/2019 6:24 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, Please check out this thread as it has a piece of code to check if you are able to read your I/Os correctly (read-di-test.zip). If this works fine, check out the updated nodes in the same thread and let us know if they work for you. Kind regards! |
Follow us on