8/19/2020 9:22 PM | |
Posts: 5 Rating: (0) |
** Sorry for the Epic Bump** I Have the same problem as Antony. I have a different version of the module SM1232. That version doesn't have the X11 so you can't mix that one up. 6ES7-232-4HD32-0XB0 AQ SM 1232 4AO +/-10V 14 BIT 0-20 MA 13 BT My channel are set to voltage and I set an output value 12000 out of 27xxx a) L+ AND M : 26.4 volts. I use Tia Portal V13 Update 9 and S7-1200 CPU 1212C DC/DC/DC V4.1 I checked connection bus via both via both I/O card. The towel is dropped.. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/20/2020 10:05:10New subject after splitting |
|
8/28/2020 12:31 AM | |
Joined: 7/7/2010 Last visit: 5/1/2024 Posts: 14661 Rating: (2350)
|
Download the hardware configuration again. While online with the PLC, what errors exist in the diagnostics buffer? See attached image for 100% fool-proof hardware update process.
|
science guy |
|
Follow us on