Industry Online Support
Technical Forum
8/28/2020 9:45 AM | |
Joined: 6/29/2017 Last visit: 8/15/2022 Posts: 1 Rating: (0) |
s7300 cpu not reading input module ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/28/2020 11:29:59New subject after splitting |
|
8/31/2020 5:58 AM | |
Joined: 12/10/2018 Last visit: 5/26/2024 Posts: 109 Rating: (11) |
Dear actautomation There are several reasons for this problem. 1. The address set for the card in the software and the hardware address must be the same. 2. The specifications entered on the card must be exactly the same as the specifications set in the HW Config. 3. The connection between the CPU and the input card should be done correctly. 4. The Input card must be live *** In such cases, the first item (the same software and hardware address) should be considered as a priority. Best regards |
Follow us on