Industry Online Support
Technical Forum
1/11/2009 3:24 PM | |
Joined: 9/27/2006 Last visit: 6/14/2024 Posts: 12260 Rating:
|
Hello manfir; First, here is a description of one fault of the CPU 313 v 1.0 corrected with new firmware versions: For the CPU313 only: - Transfer of the hardware configuration from the CPU to the PG was aborted with an error message. It is now possible to transfer the hardware configuration from the CPU to the PG. You will find the complete text of the fault corrections, along with the firmware updates available, on the following link: http://support.automation.siemens.com/WW/view/en/7345582 Unfortunately, the update procedure requires a 2MB flash card and an external prommer [or a Siemens PG with internal prommer]... Hope this helps, Daniel Chartier |
1/12/2009 4:57 AM | |
Posts: 2 Rating:
|
Thank you and I will try it. Could you tell me what is external prommer? Andwillthe program and hardware lost after I update firmware? |
Follow us on