5/29/2019 2:05 PM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Hi, the GPIOs on the IOT2000 are the same the ones from Arduino Uno Rev 3. So you can have 6 Analog Inputs. These GPIOs can be used with 3.3 or 5 V. The Siemens I/O modules does have two analog inputs, like you mentioned. BUT you use the pins on the Siemens shield with 24V instead of 3.3/5V. Best regards! |
Last edited by: Jen_Moderator at: 05/31/2019 07:59:57Added image as an attachment. Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
5/29/2019 3:15 PM | |
Posts: 2 Rating: (0) |
Thank you very much, you have helped me a lot. Sounds great. I'm going to do tests.
|