6/27/2009 11:50 AM | |
Posts: 325 Rating: (13) |
Hi, What Darius says is right. Its a thrid party tool. Regards |
6/27/2009 12:07 PM | |
Joined: 9/28/2005 Last visit: 5/23/2024 Posts: 2957 Rating: (242) |
Maybe it would be better to remove the link at least |
Best regards, |
|
6/27/2009 1:26 PM | |
Joined: 10/7/2005 Last visit: 5/29/2024 Posts: 3007 Rating: (1049) |
Before anyone decides to spend his hard earned money on some third party tools, be aware of the following: Siemens (quite cleverly) changed the way a KNOW_HOW_PROTECTED Block is compiled from the source file (from memory this was introduced with Step7 V5.3). Put simple, all comments (headers & line comments) except for the Main Block comment (which is also visible when opening a protected block) are now removed when doing a source file compilation with KNOW_HOW_PROTECT active. What this means is that if you "unprotect" aBlock in an "unorthodox way", you'll be greeted with pure code withoutcomments. KNOW_HOW_PROTECTION has also - for obvious reasons - never been a "good" way of protecting your intellectual property from being copied/stolen and used in an unauthorised way. If you need to do so (and let's face it, especially Machine OEM's really do unfortunately suffer from this), you are better off linking your program to the serial number of the memory card (see here for more on this). Bottom line is, if we would all do the "right thing" and respect other peoples work as theirs, there'd be no need for any of this (the day will probably never come but it doesn't hurt to dream does is?). |
Last edited by: fritz at: 5/10/2010 10:12 AMHave been nicely asked to remove names and links *censored* and *censored* and was happy to do so to protect the innocent, as well as avoiding them spending their money on tools that needn''t exist if we''d all do the right thing (as outlined in the original post above). Last edited by: fritz at: 6/27/2009 1:45 PMneed to remember that I finally worked out how to use auto signature... P.S: Thank you all for the nice feedback and keep up the good work. Cheers |
|
This contribution was helpful to6 thankful Users |
6/27/2009 1:35 PM | |
Joined: 9/28/2005 Last visit: 5/23/2024 Posts: 2957 Rating: (242) |
fritz, you are totally right, but I thought that posting link here is just inappropriate. |
Best regards, |
|
6/27/2009 1:39 PM | |
Posts: 8946 Rating: (999) |
Thank you, 100% Agree! Cheers, Jürgen. |
6/29/2009 1:40 AM | |
Joined: 10/7/2005 Last visit: 5/29/2024 Posts: 3007 Rating: (1049) |
Hello lalit
If this is the case then you may be able to find an old S7 project from your colleague in which the source file for the protected block still exist. If you are able to find it, then simplyremove the key word KNOW_HOW_PROTECT from it(orcomment it out by adding "//"in front of it). Once done, click on compile and the block will be unprotected (and have all comments in it too). I hope this helps |
Cheers |
|
This contribution was helpful to1 thankful Users |
5/14/2012 2:16 PM | |
Joined: 5/1/2009 Last visit: 5/23/2021 Posts: 144 Rating: (1) |
Hello so when open any blocks and display - THE BLOCK IS PROTECTED - theres no way to opening it
|
Best regard |
|
5/14/2012 8:44 PM | |
Posts: 947 Rating: (45) |
|
Follow us on