10/25/2021 5:05 PM | |
Joined: 12/1/2015 Last visit: 4/25/2024 Posts: 26 Rating: (1) |
Hello, I have similar problem using TIA v17 and startdrive 17. I have CPU s1516F-3 PN/DP and G130 CU320-2 DP + CBE20. How can I integrate this configuration in TIA v17 on profinet network? When I add everything in hw configuration, in network view I cannot connect drive with PLC using profinet. I also see the message in CU properties "with the current startdrive version operation of the communication board ethernet is only possible with the 'Sinamics link' configuration" - how can I change this to 'Profinet device'? Could anyone help me? Thank you. Update: It could help someone. This is not possible to do in Start Drive yet. But, drive can be configured from Starter and GSD file can be created and imported to TIA. This way, it works. ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 10/25/2021 19:59:05New subject after splitting Last edited by: goranv90 at: 11/09/2021 13:39:21 |
|
This contribution was helpful to2 thankful Users |