10/20/2008 1:06 PM | |
Joined: 10/15/2008 Last visit: 11/22/2023 Posts: 14 Rating: (0) |
Hy Aret, I found something interesting on this link https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=22821313&load=treecontent&lang=en&siteid=cseus&aktprim=0&objaction=csview&extranet=standard&viewreg=WW and on my case when i test a part of machine the other part are physical separated. so for each DP i should call SFC12 with LADDR corespond to the PA for that DP..? |
10/20/2008 2:23 PM | |
Posts: 2348 Rating: (263) |
Yes, you must call one time SFC12 for each slavethatisabsent. Didn't understood about PA, sorry |
10/22/2008 3:19 PM | |
Joined: 10/15/2008 Last visit: 11/22/2023 Posts: 14 Rating: (0) |
i think yes.... and that because the status of the leds is:Run green and DC green the other are off... |
10/23/2008 7:09 AM | |
Posts: 2348 Rating: (263) |
And what happends after reactivation?Isjobsuccessfull?WhatisLEDbehaviour? |
10/23/2008 2:49 PM | |
Posts: 2348 Rating: (263) |
Daniel, I agree with that. But how to find out slave's diag addr if i know DP addr INSIDE PLC programm?:^) |
10/24/2008 6:52 PM | |
Posts: 297 Rating: (41) |
You can use SFC51 to read SSL D91. The first Logadr returned is the diagnostic address. HTH, SteveA |
This contribution was helpful to1 thankful Users |
10/25/2008 12:24 PM | |
Posts: 2348 Rating: (263) |
Thanks for confimation, Steve. |
Follow us on