1/3/2022 12:48 PM | |
Joined: 1/11/2019 Last visit: 4/30/2024 Posts: 702 Rating: (140) |
Hi Ali, Point 1: The strike mark is only on Date and Time is because of miss match in or not done the time synchronization between Operator stations and PLC CPU/CPs Kindly do the time synchronization before activating the Runtime. Below link help you in configuring thr time sync (6.2.1.2 Time synchronization in a work group without central time master) SIMATIC Process control system PCS 7 Time Synchronization (V9.0 SP2) Point 2: "X" indicates that your message doe not have any comment. Point 3: "??" indicates the BATCH ID of a process (It showing as ?? Since you are not running any BATCH process). Hope all above points helps you! |
This contribution was helpful to1 thankful Users |
1/4/2022 12:45 PM | |
Joined: 4/10/2021 Last visit: 3/21/2024 Posts: 70 Rating: (6) |
Dear Techno_Taru Thanks so much for your response. Ali |